21.3.57 import_component
(Ask a Question)Description
This Tcl command imports a component *.cxf  file into the Libero project. After
                import, the *.cxf  file is placed in the
                    <project_folder>/component/work/<component_name>
                folder.
Note: Only the 
*.cxf file format is
                supported for component import.import_component -file <path_to_component.cxf> Arguments
| Parameter | Type | Description | 
|---|---|---|
| file | string | The -file argument specifies the location of the component *.cxf
                                 file to import. Both absolute and relative paths are
                                supported. | 
Error Codes
| 
                                     Error Code  | 
                                     Description  | 
|---|---|
| 
                                     None  | 
                                     Could not find the specified core file.  | 
| 
                                     None  | 
                                     Required parameter 'file' is missing.  | 
| 
                                     None  | 
                                     Parameter 'param_name' is not defined.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example imports a component my_mult.cxf file into the Libero project.
import_component -file {D:/test/my_design/my_mult.cxf}