21.3.73 remove_core
(Ask a Question)Description
This Tcl command removes a core from your project.
remove_core [-vlnv "Vendor:Library:Name:Version" ]Arguments
| Parameter | Type | Description | 
|---|---|---|
| vlnv | string | Specifies the version identifier of the core being configured. It is mandatory. | 
Error Codes
| Error Code | Description | 
|---|---|
| None | The core is not in the vault. | 
None  | The supplied name is not a valid VNLV core id: 'value'.  | 
None  | Parameter 'vlnv' is missing or has invalid value.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'remove_core [-vlnv "vlnv"]+ '  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example removes Simulation RESET_GENR from project.
remove_core -vlnv {Actel:Simulation:RESET_GEN:1.0.1}