21.3.54 get_libero_version
(Ask a Question)Description
This Tcl command returns the version number of the Libero SoC version. The value that is returned is the same as the version number that is displayed in the .
get_libero_versionArguments
| Return Type | Description | 
|---|---|
| string | Returns the version number of the Libero SoC version. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example displays Libero version number with var2 variable.
get_libero_version
#save into a variable
set var2 [get_libero_version]
#display variable
puts "Libero Version is $var2"You will see output similar to the following.
Libero Version is 12.6.0