21.3.58 import_component_data
(Ask a Question)Description
*init_reg or *init.mem files) of
                those peripherals. Use this command if and when: - The synthesized netlist or HDL files in the existing Libero SoC project contain no component (MDDR, FDDR, or SerDes) information.
 - You want to add components (MDDR, FDDR, or SerDes) into the existing design.
 
*_init.reg (register configuration file) or
                    *.mem files (memory files) can be used. Both cannot be used
                together in the same import_component_data command. import_component_data \
    -module root # name of the top_level (root) \
    -fddr file_path_and_name # has to be FDDR_init.reg or .mem \
    -mddr file_path_and_name # has to be MDDR_init.reg or .mem \
    -serdes0 file_path_and_name # has to be SERDESIF_0_init.reg or .mem \
    -serdes1 file_path_and_name # has to be SERDESIF_1_init.reg or .mem \
    -serdes2 file_path_and_name # has to be SERDESIF_2_init.reg or .mem \
    -serdes3 file_path_and_name # has to be SERDESIF_3_init.reg or .mem \
    -envm_cfg file_path_and_name # SmartFusion 2, IGLOO 2 only \
    -uprom_cfg file_path_and_name # RTG4 only
        Arguments
| Parameter | Type | Description | 
|---|---|---|
| module | string | Specifies the top level design name of the Libero project into which component data is being imported. | 
| fddr | string | Specifies the file path and file name to the FDDR_init.reg or .mem. | 
| mddr | string | Specifies the file path and file name to the MDDR_init.reg or .mem. | 
| serdes0 | string | Specifies the file path and file name to the SERDESIF_0_init.reg or .mem. | 
| serdes1 | string | Specifies the file path and file name to the SERDESIF_1_init.reg or .mem. | 
| serdes2 | string | Specifies the file path and file name to the SERDESIF_2_init.reg or .mem. | 
| serdes3 | string | Specifies the file path and file name to the SERDESIF_3_init.reg or .mem. | 
| envm_cfg | string | Specifies the file path and file name. Note: This argument is only supported for the SmartFusion® 2 and IGLOO® 2
                                    families of devices.  | 
| uprom_cfg | string | Specifies the file path and file name. Note: This argument is only supported for the RTG4™ family of devices.  | 
Error Codes
| 
                                     Error Code  | 
                                     Description  | 
|---|---|
| 
                                     None  | 
                                     Parameter 'param_name' is not defined. Valid command formatting is 'import_component_data -module "root module name" [-mddr "mddr register file name"] [-fddr "fddr register file name"] [-serdes0 "serdes0 register file name"] [-serdes1 "serdes1 register file name"] [-serdes2 "serdes2 register file name"] [-serdes3 "serdes3 register file name"] [-envm_cfg "user envm cfg file name"] [-uprom_cfg "user uprom cfg file name"]'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The component name for IGLOO 2 devices might have a different file extension
                    (*.mem or *.reg), depending on the Libero SoC
                release version used to generate the components.
The following is an example of importing design components created with a Libero SoC pre-v11.4 release into an IGLOO 2 project.
import_component_data -module <root> \
                      -fddr <file_path>/FDDR_init.mem \
                      -mddr <file_path>/MDDR_init.mem \
                      -serdes0 <file_path>/SERDESIF_0_init.mem \
                      -serdes1 <file_path>/SERDESIF_1_init.mem \
                      -serdes2 <file_path>/SERDESIF_2_init.mem \
                      -serdes3 <file_path>/SERDESIF_3_init.mem \
                      -envm_cfg <user_cfg_file_path>
            The following is an example of importing design components created with Libero SoC v11.4 or subsequent releases into an IGLOO 2 project.
*.reg file extension is
                required.import_component_data -module <root> \
                      -fddr <file_path>/FDDR_init.reg \
                      -mddr <file_path>/MDDR_init.reg \
                      -serdes0 <file_path>/SERDESIF_0_init.reg \
                      -serdes1 <file_path>/SERDESIF_1_init.reg \
                      -serdes2 <file_path>/SERDESIF_2_init.reg \
                      -serdes3 <file_path>/SERDESIF_3_init.reg \
                      -envm_cfg <user_cfg_file_path>
            The following is an example of importing design components created with a Libero SoC pre-v11.4 release into a SmartFusion 2 project.
import_component_data -module <root> \
                      -fddr <file_path>/FDDR_init.reg \
                      -mddr <file_path>/MDDR_init.reg \
                      -serdes0 <file_path>/SERDESIF_0_init.reg \
                      -serdes1 <file_path>/SERDESIF_1_init.reg \
                      -serdes2 <file_path>/SERDESIF_2_init.reg \
                      -serdes3 <file_path>/SERDESIF_3_init.reg \
                      -envm_cfg <user_cfg_file_path>
            The following is an example of importing design components created with Libero SoC v11.4 or a subsequent release into a SmartFusion 2 project.
import_component_data -module <root> -envm_cfg <user_cfg_file_path>