21.3.46 export_prog_job
(Ask a Question)Description
This Tcl command configures the parameters for the FlashPro Express programming job to be exported.
RTG4 devices do not support the security options supported by SmartFusion 2 and IGLOO 2 devices.
The syntax for the export programming job Tcl command for SmartFusion 2 and IGLOO 2 is shown below:
export_prog_job \
-job_file_name {file} \
-export_dir {absolute or relative path} \
-bitstream_file_type {TRUSTED_FACILITY | MASTER | UEK1 | UEK2} \
-bitstream_file_components {SECURITY | FABRIC | ENVM} \
-include_plaintext_passkey {0 | 1} \
-design_bitstream_format {PPD | STP} \
-prog_optional_procedures \
{action1 | procedure1 | procedure2 ; action2 | procedure1 | procedure2 | procedure3;}The syntax for the export programming job Tcl command for RTG4 is below:
export_prog_job \
-job_file_name {file} \
-export_dir {dir} \
-force_rtg4_otp {0 | 1} \
-design_bitstream_format {PPD | STP}The syntax for the export programming job Tcl command for PolarFire is below:
export_prog_job \
-job_file_name {file} \
-export_dir {dir} \
-bitstream_file_type {TRUSTED_FACILITY | MASTER | UEK1 | UEK2} \
-bitstream_file_components {SECURITY | ENVM | FABRIC | SNVM | FABRIC_SNVM} \
-zeroization_likenew_action {0 | 1} \
-zeroization_unrecoverable_action {0 | 1} \
-program_design {0 | 1} \
-program_spi_flash {0 | 1} \
-include_plaintext_passkey {0 | 1} \
-design_bitstream_format {PPD | STP} \
-prog_optional_procedures \
{action1|procedure1|procedure2;action2|procedure1|procedure2|procedure3;} \
-skip_recommended_procedures \
{action1 | procedure1 | procedure2 ; action2 | procedure1 | procedure2 | procedure3;}Arguments
| Parameter | Type | Description | 
|---|---|---|
| job_file_name | string | The name of the exported file. Name must start with design name. If omitted, design name will be used. | 
| export_dir | string | Location where the job file will be saved; any folder can be specified (absolute or release path). The default folder is the Libero designer/<design_name>/export folder. | 
| force_rtg4_otp | boolean | Enforces the use of one-time programming (OTP). This argument is optional. Valid values are: TRUE, 1, true, FALSE, 0 or false. The default value is 0. | 
| bitstream_file_type | string | Bitstream file to be included in the programming job. Only one bitstream file can be included in a programming job. Possible values are: TRUSTED_FACILITY, MASTER, UEK1, UEK2 or UEK3. If omitted, type will be TRUSTED_FACILITY. | 
| bitstream_file_components | list of components | The list of components to be included in the programming job. Components should be delimited by space. bitstream_file_components can be any one of SECURITY, ENVM, FABRIC SNVM (only PolarFire) or FABRIC_SNVM (only PolarFire) any combination of them.Note:  
  | 
| include_plaintext_passkey | boolean | Includes plaintext passkey. Valid values are: TRUE, 1, true, FALSE, 0 or false. This argument is optional. Default is 0. | 
| design_bitstream_format | string | Specifies the bitstream file formats to be exported. Space is used as a delimiter. The value can be any one of PPD, STP. If omitted, the bitstream file will be in PPD format. 
  | 
| prog_optional_procedures | string | Specifies optional procedures to program. Format: action1 | procedure1 | procedure2; action2 | procedure1 | procedure2 | procedure3; Available actions and procedures depend on the selected bitstream components. Mandatory procedures are always included. See the section Configure Actions and Procedures for supported actions and procedures. | 
| zeroization_likenew_action | boolean | Specifies that all data will be erased and the device can be reprogrammed immediately. Valid values are TRUE, 1, true, FALSE, 0 or false. Default is 0. | 
| zeroization_unrecoverable_action | boolean | Specifies that all data will be erased. The device cannot be reprogrammed and it must be scrapped. Valid values are TRUE, 1, true, FALSE, 0 or false. Default is 0. | 
| program_design | boolean | Specifies to program the design. This argument is optional. Valid values are TRUE, 1, true, FALSE, 0 or false. Default is 1. | 
| program_spi_flash | boolean | Specifies to program SPI Flash. Configure it before using. Use the Configure Design Initialization Data and Memories tool to configure it. This argument is optional. Valid values are TRUE, 1, true, FALSE, 0 or false. Default is 0. | 
| skip_recommended_procedures | string | Specifies recommended procedures to skip. Format: action1 | procedure1 | procedure2; action2 | procedure1 | procedure2 | procedure3; See the section Configure Actions and Procedures for supported actions and procedures. | 
| Return Type | Description | 
|---|---|
| integer | Returns 0 on success, 1 on failure. | 
Error Codes
| Error Code | Description | 
|---|---|
| None | bitstream_file_type: Invalid argument value: 'A' (expecting MASTER, UEK1, UEK2, UEK3 or TRUSTED_FACILITY). | 
| None | bitstream_file_components: Invalid argument value: 'A' (expecting SECURITY, FABRIC, SNVM, ENVM or FABRIC_SNVM). | 
| None | Custom security component is available for Master bitstream file only. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
SmartFusion 2/IGLOO 2
The following example exported FlashPro Express programming job in X:\12.0_Release\g4_fftousram\designer\top\export\top file. Included MASTER Bitstream file with PPD format, SECURITY and FABRIC components, plaintext passkey and specified PROGRAM, DO_VERIFY; optional procedures to program:
export_prog_job \
-job_file_name {top} \
-export_dir {X:\12.0_Release\g4_fftousram\designer\top\export} \
-bitstream_file_type {MASTER} \
-bitstream_file_components {SECURITY FABRIC} \
-include_plaintext_passkey 1 \
-design_bitstream_format {PPD} \
-prog_optional_procedures {PROGRAM | DO_VERIFY;}RTG4
The following example exported FlashPro Express programming job in X:\12.0_Release\rtg4_ff_usram\designer\top\export\top file with PPD format and also enforces the use of one-time programming (OTP):
export_prog_job \
-job_file_name {top} \
-export_dir {X:\12.0_Release\rtg4_ff_usram\designer\top\export} \
-force_rtg4_otp 1 \
-design_bitstream_format {PPD}PolarFire
The following example exported FlashPro Express programming job in X:\12.0_Release\pf_fftousram_ac_latch_launch\designer\fftousra\fftousram file. Included MASTER Bitstream file with PPD format, SECURITY, FABRIC and SNVM components, plaintext passkey and specified PROGRAM, DO_VERIFY; optional procedures to program, programs the design and device is not reprogrammed:
export_prog_job \
-job_file_name {fftousram} \
-export_dir {X:\12.0_Release\pf_fftousram_ac_latch_launch\designer\fftousram\export} \
-bitstream_file_type {MASTER} \
-bitstream_file_components {SECURITY FABRIC SNVM} \
-zeroization_likenew_action 0 \
-zeroization_unrecoverable_action 0 \
-program_design 1 \
-program_spi_flash 0 \
-include_plaintext_passkey 0 \
-design_bitstream_format {PPD} \
-prog_optional_procedures {PROGRAM | DO_VERIFY;} \
-skip_recommended_procedures {VERIFY_DIGEST | DO_ENABLE_FABRIC;}