Description
This Tcl command deletes files in your Libero SoC project.
delete_files -file {value} [-from_disk {TRUE | FALSE}]
Arguments
| Parameter | Type | Description | 
|---|
| file | string | Specifies the file you wish to delete from the project. This parameter is required for this Tcl command. It does not delete the file from the disk. | 
| from_disk | boolean | Specifies if the file will be deleted from disk or not. The default value is 'False'. This parameter is optional. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'file' has illegal value. | 
| None | Required parameter 'file' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'delete_files [-file "file"]+ [-from_disk "TRUE | FALSE"]'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
Delete the files file1.vhd and file2.vhd from the project.
delete_files -file {./project/hdl/file1.vhd} -from_disk {TRUE}