21.3.9 change_vault_location
(Ask a Question)Description
This Tcl
                command changes the location of the vault. Equivalent to clicking the Project menu,
                and choosing Vault/Repositories Setting and selecting new vault location, by default
                is "/usr/local/Microchip/common"/. The vault location is common to all Microchip
                software: 
- Project Manager
 - Firmware Catalog
 
Changing your vault location here updates the vault location for all the Microchip tools you use on your machine.
Important: This command overrides the vault
                location for all
            projects.
change_vault_location -location locationArguments
| Parameter | Type | Description | 
|---|---|---|
| location | string | Specifies the new vault location. Value must be a file path. It is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Required parameter 'location' is missing.  | 
| None | Parameter 'location' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'change_vault_location -location "location" ' .  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following command changes the old location of vault into new location.
change_vault_location -location {new_vault_path/vault}