Description
This Tcl command is intended for unsetting a global include file.
unset_global_include_file -file {filename}
Arguments
| Parameter | Type | Description | 
|---|
| file | string | The user provides the file path to unset as global include file. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Invalid Global Include File 'value'. | 
| None | Parameter 'file' has illegal value. | 
| None | Required parameter 'file' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'unset_global_include_file -file "unset global include file"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
This example unsets {./src/define.h} global include file.
unset_global_include_file -file {./prj/hdl/define.h}