21.3.75 remove_profile
(Ask a Question)Description
This Tcl command deletes a tool profile.
remove_profile -name profilenameArguments
| Parameter | Type | Description | 
|---|---|---|
| name | string | Specifies the name of the profile you wish to delete. | 
Error Codes
Error Code  | Description  | 
|---|---|
None  | Required parameter 'name' is missing.  | 
None  | Parameter 'name' has illegal value.  | 
None  | Profile 'profilename' does not exist.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'remove_profile -name "profile name"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following command deletes the profile 'custom1'.
remove_profile -name "custom1"