21.3.45 export_profiles
(Ask a Question)Description
This Tcl command exports your tool profiles. Performs the same action as the Export Profiles dialog box.
export_profiles -file { absolute path and name of exported file } \
                [-export "value" ]Arguments
| Parameter | Type | Description | 
|---|---|---|
| file | string | Specifies the absolute path and name to the exported profile file. | 
| export | string | Specifies your profile export options. The following table shows the acceptable values for this argument: 
  | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Parameter 'file' : the file '/prj/profiles_command/exp.tcl' has got an invalid extension. Valid extension is 'ini'. | 
None  | Required parameter 'file' is missing.  | 
None  | Parameter 'file' has illegal value.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'export_profiles -file "file name" [-export "predefined | user | all"] '.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following command exports all profiles to the file './profile_commands/all_profiles'.
export_profiles -file "./profile_commands/all_profiles" -export all