21.3.7 change_link
(Ask a Question)Description
This Tcl command changes the source of a linked file in your project.
change_link -file filename -path new_source_pathArguments
| Parameter | Type | Description | 
|---|---|---|
| file | string | Specifies absolute or relative path and name of the linked file you want to change. | 
| path | string | Location of the file (absolute or relative path) you want to link to. | 
Error Codes
Error Code  | Description  | 
|---|---|
None  | Required parameter 'path' is missing.  | 
None  | Required parameter 'file' is missing.  | 
None  | Parameter 'file' has illegal value.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'change_link -file "file" -path "new source path"'  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
- Change the link to a file 'sim1.vhd' in your project and link it to the c:\Microchip\link_source\simulation_test.vhd file.
change_link -file sim1.vhd \ -path {c:\Microchip\link_source\simulation_test.vhd} - Change link for the file 'test.v' from 'E:\Share\test.v' to 'E:\Share\test\srcs\test.v' using environment variable 'MSCC_ROOT_1' that has the root directory path 'E:\Share'.
change_link -file {${MSCC_ROOT_1}/test.v} \ -path {${MSCC_ROOT_1}/test/srcs/test.v}