Description
This Tcl command is for providing global include paths information.
set_global_include_path_order [-paths {“path_1” “path_2” “path_3”}]
Arguments
| Parameter | Type | Description | 
|---|
| paths | string | The user provides the list of paths to be considered as global include paths. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | One or more Global Include Paths set are invalid or do not exist. | 
| None | Invalid Global Include Path - 'value'. | 
| None | Parameter 'paths' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_global_include_path_order [-paths "[paths]+"]'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
This example considers as global include the following paths.
set_global_include_path_order -paths { “./src/GLOBAL_INCLUDE_PATH_1” “./src/GLOBAL_INCLUDE_PATH_2” “${ENV_VAR}/GLOBAL_INCLUDE_PATH_1”}