Description
This Tcl command exports the IBIS (Input/Output Buffer Information Specification) model report. The IBIS model report provides an industry-standard file format for recording parameters like driver output impedance, rise/fall time, and input loading, which may then be used by software applications such as Signal Integrity tools or IBIS simulators. The exported file has a *.ibs(name <root>.ibs) file name extension.
export_ibis_file -file {absolute or relative path and name of *.ibs file}
Arguments
| Parameter | Type | Description | 
|---|
| file | string | Specifies the absolute or relative path and name of IBIS file to export. If the file path is not specified, the file is created in <project_name>/designer/<design_name> directory. | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'file' has illegal value. | 
| None | Required parameter 'file' is missing. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following command exports the IBIS (Input/Output Buffer Information Specification) model report.
export_ibis_file -file {E:/designs/export/sd1.ibs}