21.3.88 set_global_include_file
(Ask a Question)Description
This Tcl command for setting a file as global include file.
set_global_include_file -file {filename}Arguments
| Parameter | Type | Description | 
|---|---|---|
| file | string | The user provides the file path to set as global include file. The file path can be absolute path, linked files path or path with Environment variable from project settings. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Invalid Global Include File 'value'. | 
| None | Parameter 'file' has illegal value. | 
| None | Required parameter 'file' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_global_include_file -file "set global include file"'. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example sets global include file with absolute file path.
set_global_include_file -file {E:\prj\global_include_files\hdl\add.h}ENV from Project settings
set_global_include_file -file {${ENV_2}/xyz.h}Linked Files TCL variable
set_global_include_file -file "$proj/hdl/abcd.v"