9.3.8.1 DEV_CTRL_REG Bit Definitions
| Bit Number | Name | Reset Value | Function |
|---|---|---|---|
| 7 | B-Device | 1 | Indicates whether the USB controller is operating as the A device or the B device. 0: A device 1: B device Only valid while a session is in progress. To determine the role when no session is in progress, set the session bit and read this bit. If the core is in Force_Host mode (a session has been started with TESTMODE_REG.bit[7] = 1), this bit indicates the state of the FAB_HOSTDISCON input signal. |
| 6 | FSDev | 0 | This read-only bit is set when a full speed or high speed device has been detected being connected to the port. High-speed devices are distinguished from full speed by checking for high-speed chirps when the device is reset. Only valid in Host mode. |
| 5 | LSDev | 0 | This read-only bit is set when a low-speed device is detected being connected to the port. Only valid in Host mode. |
| [4:3] | Vbus[1:0] | 0 | These read-only bits encode the current VBus level as given in Table 9-53. |
| 2 | Host Mode | 0 | This read-only bit is set when the USB controller is acting as a host. |
| 1 | Host Req | 0 | When set, the USB controller initiates the host negotiation when Suspend mode is entered It is cleared when host negotiation is completed. (B device only). |
| 0 | Session | 0 | When operating as an A device, this bit is
set or cleared by the Cortex-M3 processor (or fabric master) to start or end a
session. When operating as a B device, this bit is set/cleared by the USB
controller when a session starts/ends. It is also set by the Cortex-M3
processor (or fabric master) to initiate the session request protocol. When the
USB controller is in Suspend mode, the bit gets cleared by the Cortex-M3
processor (or fabric master) to perform a software disconnect. Clearing this bit when the core is not suspended results in undefined behavior. |