5.34.111.1 Examples
Syntax for the get_defvar command followed by a sample command:
get_defvar variable
get_defvar “DESIGN”
Syntax for the backannotate command followed by a sample command:
backannotate -name file_name -format format_type -language language -dir directory_name [-netlist] [-pin]
backannotate -dir \
{..\design} -name "fanouttest_ba.sdf" -format "SDF" -language "VERILOG" \
-netlist
timer_get_clock_actuals
Displays the actual clock frequency in the Log window, when the timing analysis tool is initiated.
timer_get_clock_actuals -clock clock_name
Deletes a probe on nets in a probed ADB file.
delete_probe –net <net_name>
Displays the actual clock frequency in the Log window, when the timing analysis tool is initiated.
timer_get_clock_actuals -clock clock_name
Restores constraints previously committed in Timer.
timer_restore
Creates a new clock or set domain.
smartpower_create_domain -domain_type {value} -domain_name {domain_name}
is_source_file_current
Audits the source file and determines whether or not the file is out of date / imported into the workspace. Returns '0' if file_name is out of date or has not been imported into the workspace, and returns '1' if file_name is current.
This command ignores the Audit settings in your ADB file.
is_source_file_current(filename)
get_defvar
get_defvar variable
Provides access to the internal variables within Designer and returns its value. This command also prints the value of the Designer variable on the Log window.
remove_min_delay
remove_min_delay [-from from_list] [-to to_list] [-through through_list] remove_min_delay -id constraint_ID
Removes a minimum delay constraint in the current timing scenario by specifying either its exact arguments or its ID.
new_design
new_design -name design_name -family family_name –path pathname–block value
Creates a new design. You need all three arguments for this command. This command will set up the Designer software for importing design source files
clone_scenario
clone_scenario name -source origin
Creates a new timing scenario by duplicating an existing one. You must provide a unique name (that is, it cannot already be used by another timing scenario).
smartpower_change_clock_statistics
Changes the default frequencies and probabilities for a specific domain.
smartpower_change_clock_statistics -domain_name {value} -clocks_freq {value} - clocks_proba {value} -registers_freq {value} -registers_proba {value} -set_reset_freq
{value} -set_reset_proba {value} -primaryinputs_freq {value} -primaryinputs_proba {value} - combinational_freq {value} -combinational_proba {value}
all_registers
Returns an object representing register pins or cells in the current scenario based on the given parameters.
all_registers [-clock clock_name]
[-async_pins][-output_pins][-data_pins][-clock_pins]
delete_files
Deletes files in your Libero IDE project.
delete_files
-file value
-from_disk
rename_library
Renames a VHDL library in your project.
rename_library
-library name
-name name
create_generated_clock
Tcl Command Documentation Conventions
remove_input_delay
remove_input_delay -clock clock_name port_pin_list
remove_input_delay -id constraint_ID
Removes an input delay a clock on a port by specifying both the clocks and port names or the ID of the input_delay constraint to remove.
st_create_set
Creates a set of paths to be analyzed. Use the arguments to specify which paths to include. To create a set that is a subset of a clock domain, specify it with -clock and -type. To create a set that is a subset of an inter-clock domain
set, specify it with -source_clock and -sink_clock. To create a set that is a subset (filter) of an existing named set, specify the set to be filtered with -from_set.
To create a set that is not derived from an existing set, you must provide both the -source pin_list and - sinkpin_list derived. Otherwise, the -source and -sink arguments act as filters on the pins from the parent set. You must give each new set a unique name in the design.
st_create_set -name name
[-parent_set name ]
[-clockclock_id -type value ] [-in_to_out]
[-source_clock clock_id -sink_clock clock_id] [-source pin_list ] -sink pin_list ]
remove_disable_timing
remove_disable_timing -from value -to value name -id name
Removes a disable timing constraint by specifying its arguments, or its ID. If the arguments do not match a disable timing constraint, or if the ID does not refer to a disable timing constraint, the command fails.
smartpower_remove_pin_probability
smartpower_remove_pin_probability –pin_name {pin_name}
Removes the probability value associated with a specific pin. This pin will have a default probability based on the domain set it belongs to.
get_design_filename
get_design_filename
Retrieves the full qualified path of the design file. The result will be an empty string if the design has not been saved to disk. This command is equivalent to the command “get_design_info DESIGN_PATH.” This command predates get_design_info and is supported for backward-compatibility.
timer_get_path_constraints
Displays the path constraints that were set as the maximum delay constraint in the timing analysis tool.
timer_get_path_constraints
save_design
save_design filename
The save_design command saves the current design in Designer to a file. If filename is not a complete path name, the ADB file is written into the current working directory.
timer_add_stop
Adds the specified pin to the list of pins through which the paths will not be displayed in the timing analysis tool.
timer_add_stop -pin pin_name
set_current_scenario
set_current_scenario name
Specifies the timing scenario for the Timing Analyzer to use. All commands that follow this command will apply to the specified timing scenario.
are_all_source_files_current
are_all_source_files_current
Audits all source files and determines whether or not they are out of date / imported into the workspace. Returns '1' if all source files are current Returns '0' if all source files are not current This command ignores the Audit settings in your ADB file.
smartpower_set_scenario_for_analysis
Sets the scenario for cycle-accurate power analysis.
smartpower_set_scenario_for_analysis -scenario{value}
smartpower_add_new_scenario
Creates a new scenario.
smartpower_add_new_scenario -name {value} -description {value} -mode {value}
remove_generated_clock
Removes the specified generated clock constraint from the current scenario.
remove_generated_clock {-name clock_name | -id constraint_ID }
smartpower_set_preferences
smartpower_set_preferences -powerunit {value} -frequnit {value} -opmode {value} -opcond
{value} -toggle {value}
Sets the following preferences: power unit, frequency unit, operating mode, operating conditions, and toggle. These preferences can also be set from the Preferences dialog box.
get_ports
Returns an object representing the port(s) that match those specified in the pattern argument.
get_portspattern
use_source_file
Defines a module for your project.
use_source_file
-file value
-module value
use_file
Specifies which file in your project to use.
use_file
-file value
-module value
-designer_view value
use_source_file
Defines a module for your project.
use_source_file
-file value
-module value
get_cells
Returns an object representing the cells (instances) that match those specified in the pattern argument.
get_cells pattern
st_edit_set
Modify the paths in a user set.
st_edit_set -name name
[-source pin_list ] [-sink pin_list ] [-rename_to name ]
list_output_delays
Returns details about all of the output delay constraints in the current timing constraint scenario.
list_output_delays
st_list_paths
Displays the list of paths in the same tabular format shown in SmartTime.
st_list_paths [-set name ]
[-clock clock_id -type value ] [-in_to_out]
[-source_clock clock_id -sink_clock clock_id] [-source pin_list ] [-sink pin_list ]
[-analysis value ] [-format value ]
generate_probes
generate_probes –save <ADB_file_name>
Executes the probing and creates a new ADB file. This command is used in conjunction with the add_probe Tcl command (see example below).
timer_commit
Saves the changes made to constraints into the Designer database.
timer_commit
set_design
set_design -name design_name -family family_name –pathpath_name
This set_design command specifies the design name, family and path in which Designer will process the design. This step is absolutely required before importing the source files.
You need all three arguments for this command to set up your design.
set_output_delay
Defines the output delay of an output relative to a clock in the current scenario.
set_output_delay delay_value -clock clock_ref [–max] [–min] [–clock_fall] output_list
st_set_options
st_set_options [-max_opcond value ] [-min_opcond value]
[-interclockdomain_analysis value] [-use_bibuf_loopbacks value]
[-enable_recovery_removal_checks value] [-break_at_async value]
[-filter_when_slack_below value] [-filter_when_slack_above value] [-remove_slack_filters]
[-limit_max_paths value]
[-expand_clock_network value] [-expand_parallel_paths value] [-analysis_scenario value]
[-tdpr_scenario value] [-reset]
Sets options for timing analysis. With no parameters given, it will display the current settings of the options. For IGLOO, ProASIC3, SmartFusion, Fusion, ProASICPLUS, and Axcelerator families, these options also affect timing-driven place-and-route.
set_defvar
set_defvar variable value
The set_defvar command sets an internal variable in the Designer system. You must specify at least one argument for this command.
timer_add_clock_exception
Adds an exception to or from a pin with respect to a specified clock.
timer_add_clock_exception -clock clock_name -pin pin_name -dir value
smartpower_edit_custom_mode
Edits a custom mode.
smartpower_edit_custom_mode -name {old_mode_name} new_name {new_mode_name} -description
{mode_description}
remove_clock_uncertainty
remove_clock_uncertainty -from | -rise_from | -fall_from from_clock_list -to | -rise_to| - fall_to to_clock_list -setup {value} -hold {value}
remove_clock_uncertainty -id constraint_ID
Removes a clock-to-clock uncertainty from the current timing scenario by specifying either its exact arguments or its ID.
create_generated_clock
Creates an internally generated clock constraint on the ports/pins and defines its characteristics.
create_generated_clock [-name name] -source reference_pin [-divide_by divide_factor] [-multiply_by multiply_factor] [-invert] source
remove_clock_latency
Removes a clock source latency from the specified clock and from all edges of the clock.
remove_clock_latency {-source clock_name_or_source |-id constraint_ID}
smartpower_remove_scenario
Remmoves a scenario from the current design.
smartpower_remove_scenario -name {value}
add_probe
Adds a probe to an internal net in your design, using the original name from the optimized netlist in your design. Also, this command must be used in conjunction with the generate_probes command to generate a probed ADB file (see example below).
You must complete layout before you use this command.
add_probe –net <net_name> [-pin <pin_name>] [-port <port_name>] [-assign_to_used_pin
<TRUE|FALSE>]
st_remove_set
Deletes a user set from the design.
st_remove_set -name name