5.34.111.5 Arguments

-net <net_name>

Name of the net you want to probe. You cannot probe HARDWIRED, POWER, or INTRINSIC nets.

-pin <pin_name>

Name of the package pin at which you want to put the net to be probed. Argument is optional; if unspecified the net is routed to any free package pin.

-port <port_name>

Name of the port you are adding. Argument is optional; if unspecified the default value is PROBE_<n>.

-assign_to_used_pin <TRUE|FALSE>

Probes a net on an already used pin. The net on the existing pin will be disconnected. Argument is optional; if unspecified the net can be only routed on unused pin.