5.34.105.24 Arguments
-logfile filename
Specifies the filename of your logfile.
-script filename
Appends any scripts you wish to add to add to the flow, where filename is the name of the script.
-append_commands commands
Appends commands (if any), where commands is the list of appended commands.
-adb value
Creates or opens your ADB file. The following table shows the acceptable values for this argument:
Value | Description |
new | Creates a new ADB file |
open | Opens an existing ADB file |
default | Uses the default ADB file in your Libero IDE project |
-compile value
Compiles your design. The following table shows the acceptable values for this argument:
Value | Description |
TRUE | Runs compile |
FALSE | Does not run compile, proceeds to the next command |
-layout value
Runs layout on your design. The following table shows the acceptable values for this argument:
Value | Description |
TRUE | Runs layout |
FALSE | Does not run layout, proceeds to the next command |
-export_ba value
Exports back-annotate files for your design. The following table shows the acceptable values for this argument:
Value | Description |
TRUE | Exports back-annotate files |
FALSE | Does not export back-annotate files; proceeds to the next command |