3.4.3.8.1.12 SOTSA – Start
Of Telegram Status for Path A
Note:
- Set to hardware-controlled read-only mode if the get_rx_telegram state
machine is active.
| Name: | SOTSA |
| Offset: | 0x092 |
| Reset: | 0x00 |
This register
displays the status of all start of telegram conditions. The corresponding bit is set to
‘1’ if the condition has matched. It is cleared if a
‘1’ is written to its position or the receiving path A is disabled
(RDPR.PRFLT = 1 or RDPR.PRPTA = 1). The flags are
handled by the hardware if the get_rx_telegram state machine is activated (SSMRR.SSMR).
In this case, the flags are cleared if an activated error condition for RDSIFR.EOTA
occurs. This is done automatically by toggling the RDPR.APRPTA
bit.
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| | WCOBO | RROA | SFIDOA | WUPOA | MANOA | SYTOA | AMPOA | CAROA | |
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Bit 7 – WCOBO Wake Check OK on
Path B OK
The bit is set at a successful
wake check OK from path B (RDSIFR.WCOB) that can be used as a precondition for a
successful wake check (RDSIFR.WCOA) and start of telegram (RDSIFR.SOTA) detection on
path A. It is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTA interrupt flag, or the
receiving path A is disabled.
Bit 6 – RROA RSSI Range OK on
Path A
This bit is set if the
received signal strength on path A is within the expected range. The RSSI comparison
is based on the first averaged RSSI sample after RX start-up. A failure of this
check is indicated by the setting of the RSSFA flag in the EOTSA register. It is
cleared if a ‘1’ is written to its position, a ‘1’
is written to the RDSIFR.SOTA interrupt flag, or the receiving path A is
disabled.
Bit 5 – SFIDOA Start of Frame
Identifier Matched on Path A
This bit indicates a
successful correlator-based start of frame ID check. It is cleared if a
‘1’ is written to its position, a ‘1’ is
written to the RDSIFR.SOTA interrupt flag, or the receiving path A is
disabled.
Bit 4 – WUPOA Wake-Up Pattern
Matched on Path A
This bit is set if the wake-up
pattern match occurred. It is cleared if a ‘1’ is written to its
position, a ‘1’ is written to the RDSIFR.SOTA interrupt flag, or
the receiving path A is disabled.
Bit 3 – MANOA Manchester Coding
OK on Path A
This bit is set if the
Manchester coding check is OK. The Manchester coding is verified for the duration
specified in the SYCSA register. If it was right for this duration, it is considered
OK. A failure of this check is indicated by the setting of the MANFEA flag in the
EOTS register. It is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTA interrupt flag, or the
receiving path A is disabled.
Bit 2 – SYTOA Symbol Timing OK on
Path A
This bit is set if the symbol
timing check is OK. The symbol timing is verified for the duration specified in the
SYCSA register. If it was right for this duration, it is considered OK. A failure of
this check is indicated by the setting of the SYTFEA flag in the EOTS register. It
is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTA interrupt flag, or the
receiving path A is disabled.
Bit 1 – AMPOA Amplitude OK on
Path A
This bit is set if the signal
amplitude inside the demodulator is above a specified threshold (DMMA.DMATA). A
failure of this check is indicated by the setting of the AMPFA flag in the EOTSA
register. It is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTA interrupt flag, or the
receiving path A is disabled.
Bit 0 – CAROA Carrier Check OK on
Path A
This bit is set by a
successful signal carrier check. A failure of this check is indicated by the setting
of the CARFA flag in the EOTSA register. It is cleared if a ‘1’ is
written to its position, a ‘1’ is written to the RDSIFR.SOTA
interrupt flag, or the receiving path A is disabled.