5.34.123.1 Arguments
-name design_name
The name of the design. This is used as the base name for most of the files generated from Designer.
-family family_name
The Microchip device family for which the design is being targeted.
-path path_name
The physical path of the directory in which the design files will be created.
block value
Enables or disables Block mode.The following table shows the acceptable values for this option:
Value | Description |
on | Enables Block mode |
off | Disables Block mode |