28.2.40 __builtin_edspage
Architecture
dsPIC33C/E/F, dsPIC30
Description
Returns the eds page number of the object whose address is given as a parameter. The
argument p must be the address of an object in an Extended Data Space (EDS); otherwise
an error message is produced and the compilation fails. See the space
attribute in Variable Attributes.
Prototype
uint16_t __builtin_edspage(const void *p);
Argument
p – literal address of an object
Return Value
Returns the eds page number of the object whose address is given as a parameter.
Assembler Operator
edspage
Error Messages
The following error message is produced when this function is used incorrectly:
“Argument to __builtin_edspage() is not the address of an object in
extended data space.”
The argument must be an explicit object address.
For example, if obj is object in an executable or read-only
section, the following syntax is valid:
uint16_t page = __builtin_edspage(&obj);