28.2.117 __builtin_sacr
Architecture
dsPIC33C/E/F, dsPIC30
Description
Shifts value by shift and returns the value which is rounded
using the rounding mode determined by the CORCONbits.RND control bit.
For example:
volatile register int16_t value asm("A");
int16_t result;
result = __builtin_sacr(value,3);
Might generate:
sac.r A, #3, w0
Prototype
int16_t __builtin_sacr(int16_t value, int16_t shift);
Arguments
value – Integer number to be shifted.
shift – Literal amount to shift between -8 and 7
Return Value
Returns the shifted result to CORCON register.
Machine Instruction
sacr
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
- the shift value is not a literal within range