28.2.131 __builtin_tbloffset
Architecture
dsPIC33C/E/F, dsPIC30
Description
Returns the table page offset of the object whose address is given as a parameter. The
argument p must be the address of an object in an EE data, PSV
or executable memory space; otherwise an error message is produced and the compilation
fails. See the space attribute in Variable Attributes.
Prototype
uint16_t __builtin_tbloffset(const void *p);
Argument
p – literal address of an object
Return Value
Returns the table page number offset of the object whose address is given as a parameter.
Assembler Operator
tbloffset
Error Messages
The following error message is produced when this function is used incorrectly:
“Argument to __builtin_tbloffset() is not the address of an object in
code, psv, or eedata section.”
The argument must be an explicit object address.
For example, if obj is object in an executable or read-only
section, the following syntax is valid:
uint16_t page = __builtin_tbloffset(&obj);