28.2.19 __builtin_divf
Architecture
dsPIC33C/E/F, dsPIC30
Description
Computes the quotient num / den. A math
error exception occurs if den is zero. Function arguments are
signed, as is the function result.
Prototype
int16_t __builtin_divf(int16_t num, int16_t den);
Arguments
num – numerator
den – denominator
Return Value
Returns the signed integer value of the quotient num /
den.
Machine Instruction
div.f