28.2.5 __builtin_addab
Architecture
dsPIC33C/E/F, dsPIC30
Description
Add accumulators A and B with the result written back to the specified accumulator.
volatile register int16_t result asm("A");
volatile register int16_t B asm("B");
result = __builtin_addab(result,B);
will generate:
add A
Prototype
int16_t __builtin_addab(int16_t Accum_a, int16_t Accum_b);
Arguments
Accum_a – First accumulator to add.
Accum_b – Second accumulator to add.
Return Value
Returns the addition result to an accumulator.
Machine Instruction
add a
Error Messages
An error message will be displayed if the result is not an accumulator register.