TCPIP_Helper_MACAddressToString Function
C
bool TCPIP_Helper_MACAddressToString(
const TCPIP_MAC_ADDR* macAddr,
char* buff,
size_t buffSize
);
Description
This function will convert a MAC address to a string representation.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| macAddr | Pointer to address to convert. |
| buff | Buffer to store the string representation. |
| buffSize | Size of the buffer. |
Returns
True - A MAC address was successfully decoded.
False - macAddr == 0 or buff == 0 or supplied buffer was not large enough or the format was incorrect.
Remarks
None.