TCPIP_STACK_NetDefaultSet Function
C
bool TCPIP_STACK_NetDefaultSet(
TCPIP_NET_HANDLE netH
);
Description
This function sets the current default network interface in the TCP/IP stack.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle. |
Returns
True - If success.
False - If failed (the old interface does not change).
Remarks
None.