TCPIP_STACK_ModuleConfigGet Function
C
size_t TCPIP_STACK_ModuleConfigGet(
TCPIP_STACK_MODULE modId,
void* configBuff,
size_t buffSize,
size_t* pNeededSize
);
Description
This function returns the current configuration data of the stack module specified by the corresponding module ID.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.
Parameters
| Parameters | Description |
|---|---|
| modId | The ID that identifies the requested module. |
| configBuff | Pointer to a buffer that will receive the configuration data. If this pointer is 0, just the pNeededSize will be updated. |
| buffSize | Size of the provided buffer. |
| pNeededSize | Pointer to an address to store the number of bytes needed to store this module configuration data. Can be NULL if not needed. |
Returns
The number of bytes copied to the user buffer:
-1 - If the module ID is invalid.
0 - If the configBuff is NULL or buffSize is less than required.
> 0 - If the call succeeded and the configuration was copied.
Remarks
Currently, only the MAC modules implement this function.
Example
uint8_t configBuffer[200];
size_t configSize;
size_t copiedSize;
copiedSize = TCPIP_STACK_ModuleConfigGet(TCPIP_MODULE_MAC_MRF24WN, configBuffer, sizeof(configBuffer), &configSize);