TCPIP_Helper_SecurePortSet Function
C
bool TCPIP_Helper_SecurePortSet(
uint16_t port,
bool streamSocket,
bool isSecure
);
Description
This function sets the internal data for deciding if the required port is a secure port or not. A secure port is one that requires secure connections. The TCP/IP internally maintained table with the ports that require secure connections is manipulated with this function. This table can be queried using the TCPIP_Helper_TCPSecurePortGet() function.
Preconditions
TCP/IP stack properly initialized.
Parameters
| Parameters | Description |
|---|---|
| port | The TCP/UDP port to set. |
| streamSocket | If true, a stream/TCP port is queried. Else, a datagram/UDP port is queried. |
| isSecure | If true, the port is set as requiring secure connection. If false, the port is set as not requiring a secure connection and it will be removed from the secure ports table. |
Returns
True - The port status successfully changed.
False - The port status could not be changed (no more slots in the table, port not found, etc.).
Remarks
Currently there is no protection for multiple threads accessing and modifying the entries in the secure port table. It is thus recommended that the updates to the table occur justs once at initialization time and after that all threads perform read-only accesses.