TCPIP_Helper_StringToIPAddress Function
C
bool TCPIP_Helper_StringToIPAddress(
const char* str,
IPV4_ADDR* IPAddress
);
Description
This function parses a dotted-quad decimal IP address string into an IPV4_ADDR struct. The output result is big-endian.
Preconditions
IP Address - a valid pointer to an IPV4_ADDR.
Parameters
| Parameters | Description |
|---|---|
| str | Pointer to a dotted-quad IP address string. |
| IPAddress | Pointer to IPV4_ADDR in which to store the result. |
Returns
True - An IP address was successfully decoded.
False - Pointer to IPV4_ADDR in which to store the result.
Remarks
If str == NULL or strlen(str) == 0, the result will be address 0.