TCPIP_STACK_NetMACStatisticsGet Function
C
bool TCPIP_STACK_NetMACStatisticsGet(
TCPIP_NET_HANDLE netH,
TCPIP_MAC_RX_STATISTICS* pRxStatistics,
TCPIP_MAC_TX_STATISTICS* pTxStatistics
);
Description
This function returns the statistics data of the MAC that's attached to the specified network interface.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Handle of the interface to use. |
| pRxStatistics | Pointer to a TCPIP_MAC_RX_STATISTICS that will receive the current RX statistics counters. Can be NULL if not needed. |
| pTxStatistics | Pointer to a TCPIP_MAC_TX_STATISTICS that will receive the current TX statistics counters. Can be NULL if not needed. |
Returns
True - If the call succeeded.
False - If the call failed (the corresponding MAC does not implement statistics counters).
Remarks
If the netH refers to an alias interface, the MAC statistics of the primary interface are returned.
Example
TCPIP_MAC_RX_STATISTICS rxStatistics;
TCPIP_MAC_TX_STATISTICS txStatistics;
TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
if(TCPIP_STACK_NetMACStatisticsGet(netH, &rxStatistics, &txStatistics))
{
// display the statistics for the internal PIC32 MAC attached to this interface
}