TCPIP_STACK_NetMulticastSet Function
C
bool TCPIP_STACK_NetMulticastSet(
TCPIP_NET_HANDLE netH
);
Description
This function sets the current default multicast network interface in the TCP/IP stack.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The selected network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle. |
Returns
True - If successful.
False - If failed (the old interface does not change).
Remarks
At stack start up, the default multicast network is the same with the default network interface. This function allows the user to change it.