TCPIP_Helper_IsPrivateAddress Function
C
bool TCPIP_Helper_IsPrivateAddress(
uint32_t ipv4Address
);
Description
This function checks if the passed in IPv4 address is a private or a routable address.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| ipv4Address | IPv4 address to check, network order. |
Returns
True - The IPv4 address is a private address.
False - The IPv4 address is a routable address.
Remarks
None.