TCPIP_STACK_NetIPv6AddressGet Function
C
IPV6_ADDR_HANDLE TCPIP_STACK_NetIPv6AddressGet(
TCPIP_NET_HANDLE netH,
IPV6_ADDR_TYPE addType,
IPV6_ADDR_STRUCT* pAddStruct,
IPV6_ADDR_HANDLE addHandle
);
Description
This function allows the listing of the IPv6 addresses associated with an interface.
Preconditions
The TCPIP_STACK_Initialize() function must have been called before calling this function. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle to set the address of. |
| addType | Type of address to request. IPV6_ADDR_TYPE_UNICAST and IPV6_ADDR_TYPE_MULTICAST supported for now. |
| pAddStruct | Structure provided by the user that will be filled with corresponding IPV6_ADDR_STRUCT data. |
| addHandle | An address handle that allows iteration across multiple IPv6 addresses. On the first call, it has to be 0; It will begin the listing of the IPv6 addresses. On subsequent calls, it has to be a handle previously returned by a call to this function. |
Returns
Non-NULL IPV6_ADDR_HANDLE - If a valid IPv6 address was found and the pAddStruct structure was filled with data.
0 - If no such interface or interface is not enabled.
Remarks
None.
Example
IPV6_ADDR_STRUCT currAddr;
IPV6_ADDR_HANDLE currHandle;
TCPIP_NET_HANDLE hNet = TCPIP_STACK_NetHandleGet("PIC32INT");
char ipv6AddBuff[44];
currHandle = 0;
do
{
currHandle = TCPIP_STACK_NetIPv6AddressGet(netH, IPV6_ADDR_TYPE_UNICAST, &currAddr, currHandle);
if(currHandle)
{ // have a valid address; display it
TCPIP_HELPER_IPv6AddressToString(&currAddr.address, ipv6AddBuff, sizeof(ipv6AddBuff));
}
}while(currHandle != 0);