TCPIP_Helper_StringToMACAddress Function
C
bool TCPIP_Helper_StringToMACAddress(
const char* str,
uint8_t macAddr[6]
);
Description
This function parses a MAC address string "aa:bb:cc:dd:ee:ff" or "aa-bb-cc-dd-ee-ff" into an hex MAC address.
Preconditions
macAddr - valid pointer to a 6 byte MAC address field.
Parameters
| Parameters | Description |
|---|---|
| str | Pointer to a colon separated MAC address string. |
| macAddr | Pointer to buffer to store the result. |
Returns
True - A MAC address was successfully decoded.
False - No MAC address could be found, of the format was incorrect.
Remarks
If str == NULL or strlen(str) == 0, the result will be address 0.