TCPIP_STACK_NetAddressBcast Function
C
uint32_t TCPIP_STACK_NetAddressBcast(
TCPIP_NET_HANDLE netH
);
Description
The function returns the network interface broadcast address. The interface should be enabled for this function to work.
Preconditions
The TCPIP_STACK_Initialize() function must have been called before calling this function. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle to get address of. |
Returns
Broadcast IP address of that interface.
0 if no such interface.
Remarks
None.