TCPIP_STACK_Initialize Function
C
SYS_MODULE_OBJ TCPIP_STACK_Initialize(
const SYS_MODULE_INDEX index,
const SYS_MODULE_INIT * const init
);
Description
This function initializes the stack. If an error occurs, the SYS_ERROR() is called and the function deinitializes itself.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| index | Index of the TCP/IP stack to be initialized. |
| init | Pointer to initialization data. It should be a TCPIP_STACK_INIT structure carrying the following data: - pNetConf - Pointer to an array of TCPIP_NETWORK_CONFIG to support - nNets - Number of network configurations in the array - pModConfig - Pointer to an array of TCPIP_STACK_MODULE_CONFIG - nModules - Number of modules to initialize |
Returns
Valid handle to a driver object, if successful.
SYS_MODULE_OBJ_INVALID, if initialization failed.
Remarks
This function must be called before any of the stack or its component routines are used.
New TCPIP_NETWORK_CONFIG types could be added/removed at run time for implementations that support dynamic network interface creation.
Only one instance of the TCP/IP stack can run in the system and the index parameter is irrelevant.
If this call is made after the stack is successfully initialized, the current TCP/IP stack object handle will be returned.