TCPIP_MODULE_SignalFunctionDeregister Function
C
bool TCPIP_MODULE_SignalFunctionDeregister(
TCPIP_MODULE_SIGNAL_HANDLE signalHandle
);
Description
This function deregisters a previous signal function. The caller will no longer be notified of stack internal signals.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_Ready. signalHandle - a valid signal handle.
Parameters
| Parameters | Description |
|---|---|
| signalHandle | Signal handle obtained from a registration call. |
Returns
True - If the operation succeeded.
False - If the operation failed (i.e, no such module, invalid handle, etc.).
Remarks
See the remarks for TCPIP_MODULE_SignalFunctionRegister().
Example
void appSignalFunc(TCPIP_STACK_MODULE moduleId, TCPIP_MODULE_SIGNAL signal)
{
// process incoming signal for the incoming module
}
TCPIP_MODULE_SIGNAL_HANDLE signalH = TCPIP_MODULE_SignalFunctionRegister( TCPIP_MODULE_HTTP_SERVER, appSignalFunc);
// when done with this signal notification
TCPIP_MODULE_SignalFunctionDeregister(signalH);