TCPIP_STACK_NetAliasNameGet Function
C
int TCPIP_STACK_NetAliasNameGet(
TCPIP_NET_HANDLE netH,
char* nameBuffer,
int buffSize
);
Description
This function returns the alias name associated with the interface handle.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle name to obtain. |
| nameBuffer | Buffer to receive the name. Could be 0 if only name size is needed. |
| buffSize | Size of the provided buffer. |
Returns
The number of characters of the interface alias name.
0 if no such interface exists.
Remarks
The aliases names are:
"eth0", "eth1", etc. for Ethernet interfaces
"wlan0", "wlan1", etc. for Wi-Fi interfaces
For alias interfaces, names will have an appended ':n', i.e.: "eth0:0", "eth0:1", wlan0:0", etc.
See the TCPIP_STACK_IF_NAME_ALIAS_ETH, TCPIP_STACK_IF_NAME_ALIAS_WLAN in tcpip.h for the aliases names. Alias interface names are at most 8 characters long.
Example
TCPIP_NET_HANDLE netH = TCPIP_STACK_IndexToNet(0);
char ifName[8];
TCPIP_STACK_NetAliasNameGet(netH, ifName, sizeof(ifName));