TCPIP_STACK_NetBiosNameSet Function
C
bool TCPIP_STACK_NetBiosNameSet(
TCPIP_NET_HANDLE netH,
const char* biosName
);
Description
This function sets the network interface NetBIOS name.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle to set name of. |
Returns
True - If the NetBIOS name of the interface is set.
False - If no such interface or interface is not enabled.
Remarks
Exercise extreme caution when using these functions to change the settings of a running network interface. Changing these parameters at runtime can lead to unexpected behavior or loss of network connectivity. The preferred way to change the parameters for a running interface is to do so as part of the network configuration passed at the stack initialization.
Example
TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
TCPIP_STACK_NetBiosNameSet(netH, myBiosName);