TCPIP_STACK_NetIsLinked Function
C
bool TCPIP_STACK_NetIsLinked(
TCPIP_NET_HANDLE hNet
);
Description
This function returns the network interface link status.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface handle. |
Returns
True - If interface exists and the corresponding MAC is linked.
False - If the interface does not exist or the link is down.
Remarks
None.