TCPIP_Helper_TCPSecurePortGet Function
C
bool TCPIP_Helper_TCPSecurePortGet(
uint16_t tcpPort
);
Description
This function checks the internal data for detecting if the required TCP port is a secure port or not. A secure port is one that requires secure connections. The TCP/IP stack maintains an internal table with the ports that require secure connections. This table can be maintained using the TCPIP_Helper_SecurePortSe() function.
Preconditions
TCP/IP stack properly initialized.
Parameters
| Parameters | Description |
|---|---|
| tcpPort | The TCP port to query. |
Returns
True - If the port is a secure connection port.
False - If port is not secure (the port is not found in the internal secure ports table).
Remarks
The TCP/IP stack populates the internal secure port table with default values as part of the stack power up procedure. The table is not re-initialized when the stack is brought down and then restarted.