TCPIP_STACK_HandlerRegister Function
C
TCPIP_EVENT_HANDLE TCPIP_STACK_HandlerRegister(
TCPIP_NET_HANDLE hNet,
TCPIP_EVENT evMask,
TCPIP_STACK_EVENT_HANDLER notifyHandler,
const void* notifyfParam
);
Description
This function sets a new event notification handler. The caller can use the handler to be notified of stack events.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_Ready. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| hNet | Network handle. |
| evMask | Mask of events to be notified of. |
| notifyHandler | The event notification handler. |
| notifyfParam | Notification handler parameter. |
Returns
A valid TCPIP_EVENT_HANDLE - If the operation succeeded.
NULL - If the operation failed.
Remarks
The notification handler may be called from the ISR which detects the corresponding event. The event notification handler has to be kept as short as possible and non-blocking.
Without a notification handler the stack user can still call TCPIP_STACK_GetPending() to see if processing by the stack needed. Currently only a primary interface can report events. The call will fail if the specified network is an alias.
Example
TCPIP_EVENT_HANDLE myHandle = TCPIP_STACK_HandlerRegister( hNet, TCPIP_EV_CONN_ALL, myEventHandler, myParam );