TCPIP_Helper_SecurePortGetByIndex Function
C
uint16_t TCPIP_Helper_SecurePortGetByIndex(
int index,
bool streamSocket,
int* pnIndexes
);
Description
This function returns the secure TCP/UDP port situated at the internal port table requested index. It also returns the number of indexes currently in the table.
Preconditions
TCP/IP stack properly initialized.
Parameters
| Parameters | Description |
|---|---|
| index | The port index to query. 0 should always be a valid index. |
| streamSocket | If true, a stream/TCP port is queried. Else, a datagram/UDP port is queried. |
| pnIndexes | Pointer to store the number of indexes that the table currently has. Could be NULL if not needed. |
Returns
A port number corresponding to the required index.
0 if the corresponding slot is free or the port is not associated with the requested stream/datagram flag.
Remarks
None.