TCPIP_STACK_NetUp Function
C
bool TCPIP_STACK_NetUp(
TCPIP_NET_HANDLE netH,
const TCPIP_NETWORK_CONFIG* pUsrConfig
);
Description
This function brings a network interface up and perform its initialization.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle. |
| pUsrConfig | Pointer to a TCPIP_NETWORK_CONFIG for the interface initialization. |
Returns
True - If success.
False - If no such network or an error occurred.
Remarks
If the interface to be brought up is a primary interface, then all its aliases remain turned down. A separate call to TCPIP_STACK_NetUp() is needed for each of the aliases.
If the interface to be brought up is an alias interface, the primary interface of this alias has to be up and running. A separate call to TCPIP_STACK_NetUp() is needed for each of the aliases.