TCPIP_STACK_NetMask Function
C
uint32_t TCPIP_STACK_NetMask(
TCPIP_NET_HANDLE netH
);
Description
This function returns the IPv4 address mask of the specified interface. If the interface is enabled then it returns the IP address mask of that interface.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle to get mask of. |
Returns
IPv4 address mask of that interface.
0 if interface is disabled/non-existent.
Remarks
None.
Example
TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
uint32_t subMask = TCPIP_STACK_NetMask(netH);