TCPIP_Helper_Base64Decode Function
C
uint16_t TCPIP_Helper_Base64Decode(
const uint8_t* sourceData,
uint16_t sourceLen,
uint8_t* destData,
uint16_t destLen
);
Description
Decodes a base-64 array to its literal representation.
Preconditions
sourceData, destData - valid pointers.
Parameters
| Parameters | Description |
|---|---|
| sourceData | Pointer to a string of base-64 encoded data. |
| sourceLen | Length of the base-64 source data. Maximum length that can be written to destData. |
| destData | Pointer to write the decoded data. |
Returns
Number of decoded bytes written to destData.
Remarks
This function will ignore invalid base-64 characters (CR, LF, etc). If sourceData is equal to destData, the data will be converted in-place. If sourceData is not equal to destData, but the regions overlap, the behavior is undefined. Decoded data size is 3/4 the size of the encoded source data.