TCPIP_STACK_NetDown Function
C
bool TCPIP_STACK_NetDown(
TCPIP_NET_HANDLE netH
);
Description
This function performs the deinitialization of a net interface. As part of this process, the corresponding MAC driver is deinitialized.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle. |
Returns
True - If success.
False - If no such network interface or the interface is already down.
Remarks
If the interface to be brought down is a primary interface, then all its aliases will be brought down as well. If the interface to be brought down as an alias interface, then other interfaces won't be affected.