TCPIP_STACK_NetAddressSet Function
C
bool TCPIP_STACK_NetAddressSet(
TCPIP_NET_HANDLE netH,
IPV4_ADDR* ipAddress,
IPV4_ADDR* mask,
bool setDefault
);
Description
This function sets the associated network IP address and/or mask. If you're chaning the network then it is preferred that you set both of these values simultaneously to avoid having the stack running with a mismatch between its IP address and mask.
Preconditions
The TCPIP_STACK_Initialize() function must have been called before calling this function. The network interface should be up and running.
Parameters
| Parameters | Description |
|---|---|
| netH | Interface handle to set the address of. |
| ipAddress | IP address to set (could be NULL to set only the mask). |
| mask | Corresponding network mask to set (could be NULL to set only the IP address). |
| setDefault | If true, the interface default address/mask is also set. |
Returns
True - If success.
False - If no such interface or interface is not enabled.
Remarks
Exercise extreme caution when using these functions to change the settings of a running network interface. Chaning these parameters at runtime can lead to unexpected behavior or loss of network connectivity. The preferred way to change the parameters for a running interface is to do so as part of the network configuration passed at the stack initialization.
Example
TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
TCPIP_STACK_NetAddressSet(netH, &myIPAddress, &myIPMask, false);