| 7 | FIER | R | 0 | This bit is set when there is at least one
parity error, framing error, or break indication in FIFO. FIER is cleared when
Cortex®-M3 processor reads the LSR, if there are no
subsequent errors in the FIFO. |
| 6 | TEMT | R | 1 | Transmit empty (TEMT). This bit is set to 1 when both the transmitter FIFO and shift registers are empty. |
| 5 | THRE | R | 1 | Transmitter holding register empty (THRE). Indicates that the MMUART_x is ready to transmit a new data byte. THRE causes an interrupt to the Cortex-M3 processor when bit 1 (ETBEI) in the interrupt enable register is 1. This bit is set when the Tx FIFO is empty. It is cleared when at least one byte is written to the Tx FIFO. |
| 4 | BI | R | 0 | Break interrupt (BI). Indicates that the
receive data is at 0 longer than a full word transmission time (start bit +
data bits + parity + stop bits). BI is cleared when Cortex-M3 processor reads
the line status register (Table 12-19). This
error is revealed to the Cortex-M3 processor when it is associated character is
at the top of the FIFO. When break occurs, only one zero character is loaded
into FIFO. |
| 3 | FE | R | 0 | Framing error (FE). Indicates that the
receive byte did not have a valid stop bit. FE is cleared when Cortex-M3
processor reads the Table 12-19. The MMUART_x
tries to resynchronize after a framing error. To do this, it assumes that the
framing error was due to the next start bit, so it samples this start bit
twice, and then starts receiving the data. This error is revealed to Cortex-M3
processor when it is associated character is at the top of FIFO. |
| 2 | PE | R | 0 | Parity error (PE). Indicates that the receive
byte had a parity error. PE is cleared when the Cortex-M3 processor reads the
Table 12-19. This error is revealed to the
Cortex-M3 processor when it is associated character is at the top of
FIFO. |
| 1 | OE | R | 0 | Overrun error (OE). Indicates that the new
byte was received before the Cortex-M3 processor reads the byte from the
receive buffer, and that the earlier data byte was destroyed. OE is cleared
when the Cortex-M3 processor reads the Table 12-19. If the data continues to fill the FIFO beyond the trigger level, an overrun
error occurs once the FIFO is full and the next character has been completely
received in the shift register. The character in the shift register is
overwritten, but it is not transferred to the FIFO. |
| 0 | DR | R | 0 | Data ready (DR). Indicates when a data byte is received and stored in the receive buffer or the FIFO. DR is cleared to 0 when the Cortex-M3 processor reads the data from the receive buffer or the FIFO. |